Cancel
Showing results for 
Search instead for 
Did you mean: 

[ISV] Similation speed

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

turning machine operation feed rate is 0.7mmpr.

Simulation speed is very slow.

If the feed value is 5000 mmpm, the simulation speed will be faster.

I want to simulate quickly even if the feed value is 0.7mmpr.

 

Where can I set it if possible?

4 REPLIES

Re: [ISV] Similation speed

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @kimies_saida

Either turn off the "Display by Time" or set it to a number larger than 0.01. set to 1 and test. This setting is under the simulation setting button.

Regards

Paul

2018-04-12 12_01_31-Simulation Settings.png

Re: [ISV] Similation speed

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Thank you.!!

Re: [ISV] Similation speed

Legend
Legend
Maybe that you did not changed from MMPM to MMPR.
G94 is mmpm and G95 is mmpr
So CSE take 0.7mmpm and this is very slow

Re: [ISV] Similation speed

Siemens Legend Siemens Legend
Siemens Legend

I use a UDE, and a simple proc in PB_CMD_before_motion,  to speed things up so I don't have to keep editing my simulation settings. (Sample feedrate is IPM ) Place the UDE on top level program, Select NORMAL for simulation based on feed rate, select TURBO to accelerate simulation. Test case reduced simulation plyback time to 8 minutes from 25 minutes...

 

 

UDE:

#-----------------------------------------------------------------
EVENT sim_override
{
POST_EVENT "sim_override"
UI_LABEL "Simulation Override"
CATEGORY MILL DRILL LATHE
PARAM command_status
{
TYPE o
DEFVAL "Active"
OPTIONS "Active","Inactive","User Defined"
UI_LABEL "Status"
}
PARAM sim_speed
{
TYPE o
DEFVAL "TURBO"
OPTIONS "TURBO","NORMAL"
UI_LABEL "Simulation Speed"
}
}

#---------------------------------------------------------------------------

 

PROC:

# Check to see if in simulation, if yes, set feed rate at post max

global mom_post_in_simulation
global mom_kin_rapid_feed_rate
global feed
global mom_sim_speed

if { [ info exists mom_sim_speed ] && $mom_sim_speed == "TURBO" && $mom_post_in_simulation == "CSE" } {
set mom_kin_rapid_feed_rate 1501
set feed 1500
}

 

Learn online





Solution Information