Cancel
Showing results for 
Search instead for 
Did you mean: 

ISV call sub program from current folder

Phenom
Phenom

Using "Simulate Machine Code File"

To simulate some of our process I am having to copy sub program files into the  machines \subprog folder

 ie "...\resource\library\machine\installed_machines\machine\cse_driver\fanuc\subprog"

Is there a way to use the same folder as the master program selected?

 

Thanks

 

Alex

NX9.0.3 Production

NX11.0.1 Testing

2 REPLIES

Re: ISV call sub program from current folder

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Alex,

 

you can set a user defined folder by setting up an env called  UGII_CAM_CSE_USER_DIR.

The overview below shows where cse is looking for ini/subprogram files.

 

 

2017-04-03 08_06_31-RE_ CSE -Simulation unter Teamcenter... findet to_ini.ini nicht_! wer kann helfe.jpg

 

Note: - location 2 wins over location 1

           - location 3 wins over location 2

 

Thomas

Re: ISV call sub program from current folder

Phenom
Phenom

Thanks Thomas

 

I had tried that, however I was not using the folder where the simulation assembly part was saved but the folder where the program I was running was saved

 

All working now

 

Alex

Learn online





Solution Information