Cancel
Showing results for 
Search instead for 
Did you mean: 

ISV error message "No possible solution for rotary axis due to axis limit" - heihain controller

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hello.

 

## Info

1. version : NX10.0.3

2. Machine type : 5axis table-table (BC)

MACHINE.png

3. Controller : heihain

4. error message

error.png

 

Someone experienced in this kind of problem could provide me some advice of what i need to do to solve this problem?

 

2 REPLIES 2

Re: ISV error message "No possible solution for rotary axis due to axis limit" - heihain c

Gears Phenom Gears Phenom
Gears Phenom

hello,

if we can trust this message:

1.print screen your kinematic settings and axis vectors here from your postprocessor

2.we need to see path of your operation which gives you these errors. attach files

Maybe your operation is not reachable by this kinematics.

 

- then people will have better chances to help

 

(maybe your machine model kinematic definition is wrong, I dont know)

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: ISV error message "No possible solution for rotary axis due to axis limit" - heihain c

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Try this -

Open up the rotary axes to full 360 degree rotation

post & see what values are output - see which operations exceed the actual axis limits, and what the values are.

then reset back to actual limits

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information