Cancel
Showing results for 
Search instead for 
Did you mean: 

ISV mill turn material removal

Creator
Creator

I am having trouble with an ISV machine not simulating material removal properly and I would like to know why it is happening. If my operations are turning only it works, if my operations are milling only it works, but if I use turning and milling it doesnt.

 

My reseller has not been able to diagnose it so I am opening it up the good folks here at Siemens to see if it can be fixed. 

 

Where should I start?

 

Regards

Adrian 

2 REPLIES 2

Re: ISV mill turn material removal

Siemens Legend Siemens Legend
Siemens Legend

Hi @Adrian_Black,

 

which NX version you are using currently and how you defined the geometry view for the turning and milling workpiece?

May a good starting point is also to compare to the sim15 OOTB millturn machine tool.

 

Best regards

Thomas

Re: ISV mill turn material removal

Creator
Creator

HI @ThomasJ 

I am using, NX 12.0.2.9.

Sim 015 works perfectly for me, I had been experiencing IPW problems which have now been resolved by using a geometry tree like this, but it doesnt work in simulation.

 

 

Learn online





Solution Information