Cancel
Showing results for 
Search instead for 
Did you mean: 

[ISV] simulation error in sie15 millturn machine type.

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi

 

I made the 3+2axis milling operation and tried simulation.

The order of operation generation is as follows.

 

order1.jpgorder2.jpgorder3.jpg

 

I tried simulation verification with sim15_millturn_9ax equipment.

B axis is output as minus value and does not match the machining plane direction.

 

order4.jpg

 

 

What is the problem?

 

 

1 REPLY

Re: [ISV] simulation error in sie15 millturn machine type.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Kimes,

 

what I can see it looks almost correct, hard to say what is wrong.

Please make sure and double check if the tool axis of the operation is parallel to the Z axis of the MCS POCKET-1.

 

At the end it looks strange that the B axis is -90 at all, which NX version are you using?

Can you check with the latest CCF G68.2 my have been updated.

 

For that swiveling cycle need to have the right kinematic chain set.
The variable GV_strSwivelingChainName I assume should be "B-HEAD-MAIN-SPINDLE"

 

Hope that gives some direction to check.

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information