Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

If no toolchange don't output in Post

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello all,

I don't want output S...M03...M08 if no toolchange. How can I do it. Please help!!!

Untitled.png

4 REPLIES 4

Re: If no toolchange don't output in Post

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You usually force the output of these when a tool change occurs, with MOM_force in the tool change event.

You mark them in the rapid move as optional, so that you need to force their output as described above.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: If no toolchange don't output in Post

Phenom
Phenom

As Stefan noted - modal behavior and forcing should achieve what you are after. Indication that the rapid event is the first out of a tool change (should you need it) is possible by checking:

 

if {$mom_current_motion == "initial_move"} {

NX12.02
Windows 10 Pro
ITC Inc.

Re: If no toolchange don't output in Post

Siemens Genius Siemens Genius
Siemens Genius

Also check to make sure they are being force out because of custom command in the "Start of Path" event look inside the command PB_CMD_start_of_operation_force_addresses

 

   MOM_force once S M_spindle X Y Z fourth_axis fifth_axis F

 

Will cause a Sxxxx M0x be outputted even if there is no change

Frank Bartucci
NX CAM COE

Re: If no toolchange don't output in Post

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

it's ok now, Thanks all!!!

Learn online





Solution Information