Cancel
Showing results for 
Search instead for 
Did you mean: 

Import Angular Head into Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

 

How can I import Angular Head into Teamcenter Environment. Entire machine are imported but I don't know how should I import this device. Maybe someone can help me?

 

Best regards

Bernard Pacula,
CAMdivision Sp. z o.o.
Consultant PLM/System Architect
4 REPLIES 4

Re: Import Angular Head into Teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Basic technique for any of the "text" libraries (machines, devices, tools, etc.)

 

Item ID of top level component must equal the LIBREF column entry.

 

So if the libref in the device_database.dat is "sim16_AC-Head" (to pick one of the existing devices), then the item ID of the top level part in the assembly, when loaded into TC, *must* be "sim16_AC-Head" (not sure about case sensitivity)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Import Angular Head into Teamcenter

Hi,

 

You need to import the part in TC. Best is to use the NCMachine item type for the components and assy. After that, you have to classify the head in the devices -> head. The holding system is important for the simulation (head change program). See pic. If you need more info, just let me know.

 

Brs, Niek

 

 

Re: Import Angular Head into Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thank You - can I have one more question?

If You want to import Machine to classification (for Machine Simulation in NX CAM) then how can i do this? I don't know how it is possible to attach configuration file to Machine. If there is only machine with name and description then allways I have an error when using Retrieve Machine from Library

MCHINE_ERROR.pngCLASSIFICATION_MACHINE.png

Best regards

Bernard Pacula,
CAMdivision Sp. z o.o.
Consultant PLM/System Architect

Re: Import Angular Head into Teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you set up the machines in native NX too?

You will just have to use the DAT file entry from the machine_database.dat file without the variable pointing to the installed machines folder.

# native machine_database.dat entry
${UGII_CAM_LIBRARY_INSTALLED_MACHINES_DIR}DMU_125_FD4\DMU_125_FD4.dat

# entry for the PP attribute of the machine classification
DMU_125_FD4\DMU_125_FD4.dat

Hope this helps.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information