Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Importing multiple .stp files at once?

Legend
Legend

I often use file>open> an open .stp files instead of importing them into an open file. Is there a command line line program that can open all .stp within a driectory, and save them as a .prt file. I have a lot of files to import and am not able to find a way other than opening each individually.

 

Thanks

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM
15 REPLIES 15

Re: Importing multiple .stp files at once?

Phenom
Phenom

Start-> Seimens NX -> STEP AP214 (or AP203)

 

Select import

 

Browse to directory

Re: Importing multiple .stp files at once?

Legend
Legend

Thank you. I rember seeing those, dont know why I didnt think of it. When I open I see this message. Any idea what I should point to? I tried setting  set UGII_JAVA_HOME_DIR=C:\Program Files\Java\jre1.8.0_45\bin\ in the ugii_env.dat., and I still get the same message.

 

 

JAVA.PNG

 

 

 

 

 

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Re: Importing multiple .stp files at once?

Phenom
Phenom

It normally works without editing any variables.

It could be a 32 64 bit problem.

It looks like you are pointing to the 64bit JRE

Have you installed the 32bit JRE?

 

alternatively save the following as a .bat file and drag and drop step files onto batch file, imported files will be in same location a step files. not sure if this works will NX11 as directory names have changed ugii -> NXBIN

 

@echo off
:: if multiple versions installed uncomment 
:: line below and edit to version folder required

::set UGII_BASE_DIR=C:\UG\NX9

set UGII_ROOT_DIR=%UGII_BASE_DIR%\ugii
set PATH=%UGII_ROOT_DIR%;%PATH%
set STEP214UG_DIR=%UGII_BASE_DIR%\step214ug\
set ROSE_DB=%STEP214UG_DIR%
set ROSE=%STEP214UG_DIR%

:Loop
if '%1'=='' goto DONE
call "%STEP214UG_DIR%\step214UG.exe" %1
shift
goto Loop

:DONE

 

Re: Importing multiple .stp files at once?

Legend
Legend

Thanks, that seemed to work perfectly. I just dragged a group of .stp files onto the new batch file. Part files were created in the original directory along with all the sub components of the assemblies.  

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Re: Importing multiple .stp files at once?

Legend
Legend
Seems to work fine in NX11, no editing required.

I tried to edit it for use with Iges as but thats not working. Is there something else iges needs?
Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2019 r1
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: Importing multiple .stp files at once?

Legend
Legend
You modified directories and .exe trying to get it to work? Does it give an error message?
Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Re: Importing multiple .stp files at once?

Legend
Legend
@echo off
:: if multiple versions installed uncomment 
:: line below and edit to version folder required

::set UGII_BASE_DIR=C:\UG\NX9

set UGII_ROOT_DIR=%UGII_BASE_DIR%\ugii
set PATH=%UGII_ROOT_DIR%;%PATH%
set IGES_DIR=%UGII_BASE_DIR%\iges\
set ROSE_DB=%IGES_DIR%
set ROSE=%IGES_DIR%

:Loop
if '%1'=='' goto DONE
call "%IGES_DIR%\iges.exe" %1
shift
goto Loop

:DONE

iges error.png

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2019 r1
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: Importing multiple .stp files at once?

Legend
Legend

I took your code for the iges and used my NX11 directory. I get a different error. I am in windows 10error_iges_open.png

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Re: Importing multiple .stp files at once?

Phenom
Phenom

In NX11 ugii folder has changed to nxbin.

 

below works for NX11

 

 

@echo off
:: if multiple versions installed uncomment 
:: line below and edit to version folder required
:: set UGII_BASE_DIR=C:\UG\NX11

:: for NX10 and below UGII_ROOT_DIR is ugii
:: for NX11 UGII_ROOT_DIR is nxbin
set UGII_ROOT_DIR=%UGII_BASE_DIR%\nxbin set PATH=%UGII_ROOT_DIR%;%PATH% set IGES_DIR=%UGII_BASE_DIR%\iges\ set ROSE_DB=%IGES_DIR% set ROSE=%IGES_DIR% :Loop if '%1'=='' goto DONE call "%IGES_DIR%\iges.exe" %1 shift goto Loop :DONE

 

Learn online





Solution Information