Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

In 12.0.2 I am unable to select convergent body for part.

 The What's New doc says it is supported in 12.0.2 but I am unable to select convergent bodies for part.  Has anyone tried it?

NX 12.0.2
4 REPLIES 4

Re: In 12.0.2 I am unable to select convergent body for part.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is this in an operation?

If so, what type?

 

Or is this in a geometry parent (Geometry View object)?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: In 12.0.2 I am unable to select convergent body for part.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi all,

 

this is a known issue and simply a bug. It will be fixed with NX12.0.2 MP2, which will be available at the 18th of September. Then you will be able to select Convergent as well as Facet bodies again in Part and Blank geometry.

 

Sorry for the inconvinience guys!

 

Cheers,

Alexander

 

 

Lead Product Manager - Mold & Die

Re: In 12.0.2 I am unable to select convergent body for part.

I wasn't aware facet body selection was bugged too, thank you for pointing that out.  I will have to install 11.0.2 if I need it before MP02 is available.

 

NX 12.0.2

Re: In 12.0.2 I am unable to select convergent body for part.

Siemens Phenom Siemens Phenom
Siemens Phenom
NX12.0.1 it works, so you don't have to jump back to NX11.0.2 :-)
Lead Product Manager - Mold & Die

Learn online





Solution Information