Cancel
Showing results for 
Search instead for 
Did you mean: 

In Post Builder, unable to inherit ude from a post.

In Post Builder I am unable to inherit ude from a post.  When I click on the Other Data Elements tab I receive an error and cannot go further.  At first I thought my posts were the problem but I also tried one of the OOTB posts and it gives me the same error.  I am running 11.0.2 mp01.

 

Could someone try do this and let me know if you experience the same error?

 

Here are the two errors I am seeing:

 

error-2.pngerror-1.png

NX 12.0.2
2 REPLIES

Re: In Post Builder, unable to inherit ude from a post.

Valued Contributor
Valued Contributor

Hi. You are not alone. I have the same problem. 

The data that is not allowed to reach coud be setted in .def file of your post.

 

FORMATTING
{
WORD_SEPARATOR " "
END_OF_LINE ";"
SEQUENCE sequence_number 1 1 1 9999

 

I think this is some problems with the post templates contained in  \POSTBUILD\pblib

I also could not create the generic turn post.  

Re: In Post Builder, unable to inherit ude from a post.

After I posted this topic I believe I found an existing PR for this problem. I don't recall which version started having the issue but the current version certainly has it.

The PR stated the work around is to click on Program & Tool Path-Word Summary-Other Data Elements to access it.
NX 12.0.2

Learn online





Solution Information