Cancel
Showing results for 
Search instead for 
Did you mean: 

Information window not resetting to start of output

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Something I just noticed in NX11.0.2

When post processing, the Information window does not reset to the start of the file every time.

 

So I start NX, open a file, post the program. When I exit the information window and post again or open another file and post, the information window does not reset back to the start of the output but to the end.  This must be related to the “new” format of the information window.

 

I have submitted and IR and it is a PR that has already been reported. PR Number 8982010

If you find this as annoying as I do, you can contact GTAC and get linked to this PR.

“The squeaky wheel gets the grease”

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Learn online





Solution Information