Cancel
Showing results for 
Search instead for 
Did you mean: 

Internal error when trying to import tool with tracking points

Genius
Genius

Happy New Year all!

 

Just wanted to see if anyone else has experienced problems when trying to load a form tool or other type that has tracking points defined from the tool_database.dat file?

If I remove the reference to the tracking point by manually altering the files I can load the tool without issue but even if I try and update the loaded tool and add new tracking points, the next time I try to use it I get the Internal Error alarm and can't close NX I have to kill it via task manager?

 

Will raise a PR but wanted to see if this has been seen before.

 

 

Regards

Dave
NX10.0.3MP13
NX11.0.1
Production
TC10
Vericut 7.3,7.4.1,8.0.2
2 REPLIES 2

Re: Internal error when trying to import tool with tracking points

This does not sound familiar to me.

As long as you are manually editing the files, take a look and be sure that the tracking point libref (such as TP001_00001) on the end of each form tool record in tool_database.dat is defined in the trackpoint_database.dat file.

 

tool_database.dat:

DATA | ugt0251_011 | 02 | 51 | ...  | TP001_00010

 

trackpoint_database.dat:

DATA | TP001_00010 | 1 | 0 | OD_TANGENT | 1 | ...
DATA | TP001_00010 | 1 | 0 | ID_TANGENT | 2 | ...
DATA | TP001_00010 | 1 | 0 | SHARP_CORNER | 3 | ...

Mark Rief
Retired Siemens

Re: Internal error when trying to import tool with tracking points

Genius
Genius
Hi Mark,
Thank you for the reply, all the references are correct I have a couple of extra references to tracking points on tools that have no tracking points defined?
GTAC are looking into my files at the moment.
Regards

Dave
NX10.0.3MP13
NX11.0.1
Production
TC10
Vericut 7.3,7.4.1,8.0.2

Learn online





Solution Information