Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Transfer motion between two operation

Legend
Legend

Will see, maybe it will have the options to turn that on and off in dialog. I can also see the possible need to control it differently between different operations. 

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Re: Transfer motion between two operation

Siemens Phenom Siemens Phenom
Siemens Phenom

@Juraj, your input is heard and we see value in it. 

 

As this feature will continue in development, we will add functionality and our customers are driving these developments.

Lead Product Manager - Mold & Die

Re: Transfer motion between two operation

Legend
Legend

Ive always thought this feature is more of a good concept but a poor reality. I'd be interested to see cycle time of full retract and reposition vs this interpolated move from operation to operation.

 


Dennis Rathi
Creations Unlimited

Re: Transfer motion between two operation

Gears Phenom Gears Phenom
Gears Phenom

@Dstryr agree, but possibility turn on interoperation path (generated in clearence geometry) would be good.

 

In particular if transfer move between operation will be 3 straigth lines (along bounding box clearence) - there will not be linearization. So it could be fast.

If clearence geometry will be spherical some machine may not handle it in rapid feedrate but some machines will.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information