Cancel
Showing results for 
Search instead for 
Did you mean: 

Invitation to support ER - allow changing inheritance of multiple ONT objects

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NX supports inheriting of parent settings, but currently one can only change that for one selected object in the ONT and not for multiple selected objects.

Below find a proposal for allowing changing the inheritance for multiple selected objects.

          ER Template
          ===========
1. Short Description of desired enhancement: <Problem rather than a solution> 
   + it is not possible to check inheritance if multiple objects are selected in the ONT
2. What activity in your process is the product not able to currently handle? 
   + we want to enable inheritance of parent settings of multiple selected CAM objects
3. What result are you trying to achieve? (Please provide as many details as possible.) 
   + for example, change inheritance of feed and speed settings of multiple operations in one go
   + bulk edit of CAM object settings in general
4. Do you currently have a workaround? 
   + change the inheritance one object after the other, which is very cumbersome if there are many
5. Do you have a proposal for the solution you envision Siemens PLM providing for this capability? 
   + enhance the existing parent settings inheritance
6. What is the level of productivity gained from such an enhancement? 
   + HIGH, allow bulk editing of settings that can be inherited from the parent
7. Other information: 
   + Link us to ER#9360786

Hope this will allow a step forward to bulk editing of objects.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information