Cancel
Showing results for 
Search instead for 
Did you mean: 

Invitation to support ER - use custom cut methods to set the HSC mode of CYCLE 32

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

From my point of view more people are suffering from the issue that it is not possible to utilize custom cut methods to set the HSC mode of CYCLE 32, when using Post Configurator.

Sure you can use the CYCLE 32 UDE, but the cut methods are already there, so why use an UDE?

Below find a proposal for a "me too" report at GTAC.

                            ER Template
                            -----------

* Short Description of desired enhancement: <Problem rather than a solution>
    - it is not possible to use custom cut methods to drive the HSC mode of CYCLE 32 for Heidenhain Post Configurator post.processors

* What activity in your process is the product not able to currently handle?
    - we want to set HSC mode based on our own cut methods, not just the two OOTB ones

* What result are you trying to achieve? (Please provide as many details as possible.)
    - have Post Configurator base the HSC mode of CYCLE 32 on our own cut methods

* Do you currently have a workaround?
    - No

* Do you have a proposal for the solution you envision Siemens PLM providing for this capability?
    - allow adding a list of cut methods for roughing
    - finishing seems to be the default, so no list needed for that

* What is the level of productivity gained from such an enhancement?
    - HIGH, better support the customers configuration and needs

* Other information:
    - Link to existing ER 9362093

Hope to get some supporters to make our lives easier in the future.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information