Cancel
Showing results for 
Search instead for 
Did you mean: 

Irregular stock in cavity mill

Builder
Builder
When i put stock 0.1 mm as part stock( wall-floor same)
As a result i got the 0.1 is wall stock and 0.3 is floor stock which is occurring problem during machining in up coming next operation
Please suggest

Thanx
7 REPLIES

Re: Irregular stock in cavity mill

Sounds like a bug.  What version of NX are you using?  If you are using an old version it is possible it works fine in another version.  Can you upload a prt file?

NX 12.0.2

Re: Irregular stock in cavity mill

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Have you changed something in "Cut Levels"?

Make sure if problem still exists if you reset Cut Levels by changing "Range Type" option to "Automatic"

...and I agree that it would be the easiest if you upload PRT file

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Irregular stock in cavity mill

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
  1. make sure to enable "use side as floor" for the stock option
  2. make sure to use automatic cut levels to get a level on each face that is perpendicular to the tool axis

If you use one range only, you will not have a level on each floor face that is perpendicular to the tool axis.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Irregular stock in cavity mill

Builder
Builder
Im using NX 10

Re: Irregular stock in cavity mill

Builder
Builder

See th eprogram name of

01_12f

please change file extension from .pdf to .prt

 

Re: Irregular stock in cavity mill

As Marek and Stefan have said, you need to set your cut levels to Automatic so NX sees the range s (floors) properly.  To do this go to cut levels and set the range type to automatic.  You can go to the list and delete the last range if you want because it will save some time when you generate the operation.  You will notice the range type now says user definied if you deleted the last cut range and this is normal.  If you use single for range type then NX is not looking at the floors.Also, in case you missed it, the tool is not cutting the floor at Z-6.8mm because it cannot fit. I would have uploaded a prt file for you but I am working with versions 11 and 12 so you would not be able to open it in version 10. 

 

Image 1.png

NX 12.0.2

Re: Irregular stock in cavity mill

Builder
Builder
Thanks to all of guys
#Mould_United
#Marek_Pawlus
#Stefan_Pendl

Learn online





Solution Information