Cancel
Showing results for 
Search instead for 
Did you mean: 

Is Show Thickness by Color still available?

Is the old Show Thickness by Color still available to use?  I seem to recall when I upgraded to 11.0.2 it was still availble although now I cannot find it.  The reason I am asking is because I am getting different results in 11.0.2; much more erroneous display of excess stock to the point where Analyze is almost unusable to me.  Adjusting thickness ranges seems to only affect the real excess stock and not the erroneous stock that is shown.    The old Show Thickness would be a workaround until this issue in Analyze gets fixed.

NX 12.0.2
4 REPLIES 4

Re: Is Show Thickness by Color still available?

Legend
Legend
Did you search in command finder for it?
Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Re: Is Show Thickness by Color still available?

Yes, I did. No result for it.

NX 12.0.2

Re: Is Show Thickness by Color still available?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Re: Is Show Thickness by Color still available?

I was hoping that wasn't the case because currently the result is not usable for 3D machining.  I have been adjusting various tolerances to obtain better results but so far have been unable to improve it.

 

I really don't want to go backwards to 11.0.1 but will if I have to because purchasing Vericut to make up for regression in 11.0.2 is not an option for us.

 

 

NX 12.0.2

Learn online





Solution Information