Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a way to point the tool axis either toward or away from a curve in NX?

PLM World Member Creator PLM World Member Creator
PLM World Member Creator

I know you can use the Tilt Tool axis after a toolpath has been generated, but I want to keep my tool axis through a curve while the toolpath is being generated.

4 REPLIES 4

It depends on which operation you are using. If you are c...

It depends on which operation you are using.

If you are cutting in levels, then take a look at ZLEVEL_5AXIS. Here you can tilt the tool axis toward or away from a point or curve.

Mark Rief
Retired Siemens

Re: It depends on which operation you are using. If you are c...

PLM World Member Creator PLM World Member Creator
PLM World Member Creator
Mark, thanks! It sure would be nice to do this on any 5 axis toolapth. ZLevel_5Axis is nice, but I don't think it allows you to machine undercuts. I now have ER Number 7120223 open for this enhancement. It's a function that many other CAM systems have and have had for sometime. It is a very useful way to control the tool axis.

Re: It depends on which operation you are using. If you are c...

You are correct - Zlevel 5 axis first creates a path by looking down the reference tool axis, so the undercuts are not seen. Then the path is tilted based on the tilt direction.

For a zlevel type path on an undercut area, you need to use another operatation type, such as surface contouring, where you can project towards the part, instead of down a fixed axis.
Mark Rief
Retired Siemens

Re: It depends on which operation you are using. If you are c...

PLM World Member Creator PLM World Member Creator
PLM World Member Creator
Mark, yes and hence I would like to control the tool axis through a curve using any other multiaxis toolpath operation. Let me know if you'd ever like to chat about this as I can show you numerous cases where this is useful.

Thanks

Jerry

Learn online





Solution Information