Cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with lathe grooving tool at and angle - Tracking point

Pioneer
Pioneer

Hi,

 

I have an angular rectangular groove to be turned. Eg: Width 8mm and depth 12 mm with .8CR.

I wanted to define the tracking point in NX the same way as we establish tool datum on the machine. (Please find attached image)

 

However, in NX I could find only the option to define the tracking point with respect to any one of the two corner radii.

 

I was wondering if there is a way to define the virtual intersection of both the extreme tangent points of the tool in X and Z axis?

 

Many Thanks,

Jithesh

NX9.0.2.5

3 REPLIES 3

Re: Issue with lathe grooving tool at and angle - Tracking point

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Can't be done as of now (12.0.1).

I'm pretty sure there's an ER, but I can't seem to find the number right now.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Issue with lathe grooving tool at and angle - Tracking point

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

 meant to say - this is also useful on a "C" insert when you're using the 100 degree angle.

 

Also, most machines (that I've encountered) allow you to touch the tool off at a "normal" position (B0/90/180, depending on the machine) then rotate the tracking point to the angle needed (although if you don't have a B axis, this won't work...)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Issue with lathe grooving tool at and angle - Tracking point

Pioneer
Pioneer

Thank you for your reply Ken !

 

I am trying to do an operation at 30 degree...

 

Best Regards,

Jithesh

Learn online





Solution Information