Cancel
Showing results for 
Search instead for 
Did you mean: 

Lack of memory in the manufacturing module NX8.5, NX9 and NX10 when the license is borrowed

Experimenter
Experimenter

Hi everibody:

 

I,m a teacher in a technical school and often I have to work out of our organization network where our license is located. The problem becames when I,m working using a borrowed license (only in the manufacturing module)and  in a short period of time computer´s memory collapse. It dosn´t mather the kind of computer after one hour the project gets blocked. Some suggestion??

6 REPLIES

Re: Lack of memory in the manufacturing module NX8.5, NX9 and NX10 when the license is borrowed

Ken_A 1st Gear
1st Gear

Sounds like a bug.

Have you reported it to GTAC?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
Apparently I've turned into a gearhead


Re: Lack of memory in the manufacturing module NX8.5, NX9 and NX10 when the license is borrowed

The license borrowing should not make a difference. 

 

Are you saying if you run on the same computer inside your network, you do not have the issue?

 

Is the computer a supported platform? How much memory does it have?

Mark Rief
Retired Siemens

Re: Lack of memory in the manufacturing module NX8.5, NX9 and NX10 when the license is borrowed

Experimenter
Experimenter

thanks

 

I will report to Gtac and post the solution if they give me one

 

 

Re: Lack of memory in the manufacturing module NX8.5, NX9 and NX10 when the license is borrowed

Experimenter
Experimenter

.

There is a big diference:

 

 

Same computer with the server license no problem but when this license is borrowed...

 

Some ratios

 

memory of 4Gb 30-45 min.

 

memory 6Gb 45-60min.

 

memory 16Gb similar a s 6Gb

 

After this time the memory is collapsed and you can see after starting the project that the use of memory starts growing and growing

 

Thkx in advance

Re: Lack of memory in the manufacturing module NX8.5, NX9 and NX10 when the license is borrowed

Ken_A 1st Gear
1st Gear

Sounds like there is a leak in the "borrowing" code...

Definitely report this to GTAC and get a IR/PR number.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
Apparently I've turned into a gearhead


Re: Lack of memory in the manufacturing module NX8.5, NX9 and NX10 when the license is borrowed

Experimenter
Experimenter

no GTAC response yet and thinking to use a VPN option, there is another aspect that I´ve realized, if I travel with my laptop turned on from my company It works perfect. I can´t understand If the borrowing option is not reliable how it is offfered.

 

lessons finished in September I hope ...

Learn online





Solution Information