Cancel
Showing results for 
Search instead for 
Did you mean: 

Lathe Trepanning

Valued Contributor
Valued Contributor

Is it Possible to configure a 2 insert trepanning tool similar to the one attached and if you can do you use a drilling cycle or do you have to use a grrving tool with 1 insert and double feed rate.

Mike

NX 11.0.2.7
Win 10
2 REPLIES 2

Re: Lathe Trepanning

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Another option would be to use a form tool and teach mode

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Lathe Trepanning

Valued Contributor
Valued Contributor

Thanks Ken,

I used teach mode as a single insert for simulation will configure tool correctly before running project as it will be a special diameter

Mike

NX 11.0.2.7
Win 10

Learn online





Solution Information