Cancel
Showing results for 
Search instead for 
Did you mean: 

Link other posts

Pioneer
Pioneer

Hello all,

 

I try to link two post to each other, I do the process in post builder-Program & Tool Path-Linked Posts,

 

And also i added operator message in post builder-Start of Path and also i defined Head UDE in NX-CAM, then i post it but it doesn't work, i added all the photos about the details,

 

Can anyone help me about this issuetorna.pngmillturn.pnglink other post.png

3 REPLIES 3

Re: Link other posts

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

The HEAD UDE needs to be attached to a Method group.  You may be able to use other group objects, I have always used the Method to get it to work.  Perhaps other can chime in with more info.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Link other posts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes, the HEAD must be attached to something OTHER than an operation.

"Method" objects are the usual ones, but they can be attached to geometry, machine tool or "folders" in the program order view.

 

Start of proc MOM_head{}:

global mom_sys_in_operation
if { [info exists mom_sys_in_operation] && $mom_sys_in_operation == 1 } {
      global mom_operation_name
      CATCH_WARNING "HEAD event should not be assigned to an operation ($mom_operation_name)."
return
}
Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Link other posts

Pioneer
Pioneer

Thank you, it works now.

Learn online





Solution Information