Cancel
Showing results for 
Search instead for 
Did you mean: 

Linked body in CAM Template

Valued Contributor
Valued Contributor

Hi all,

 

When starting a new project I create the CAM file and then create a Linked body of the CAD part.

Is it possible to implement this in the template so I don't have to do this myselve every time?

 


Regards,
Sven

NX11.0.1
2 REPLIES

Re: Linked body in CAM Template

Templates can create the assembly, but not the linked body.

Mark Rief
Retired Siemens

Re: Linked body in CAM Template

Esteemed Contributor
Esteemed Contributor

You can have the linked body ready in the template part, so you only have to select the new target body.

There is more benefit if the new target part file is saved as from the previous part file, so the CAM objects, that depend on faces and edges will be updated to use the new geometry.

Example:

  1. target part is a template for a specific piece part
  2. CAM template uses that CAD template
  3. new target part is derived from the CAD template
  4. most of the faces and edges of the linked body get matched
    • in certain cases one needs to use the replacement assistant for the matches

More or less similar to a CAM template for a part family member.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Learn online





Solution Information