Cancel
Showing results for 
Search instead for 
Did you mean: 

Looking at posted code in Teamcenter

Gears Phenom Gears Phenom
Gears Phenom

I submitted an IR to get info on this, but hoping maybe some of the CAM users can help.

 

Our machine shop creates CNC code, which is saved in Teamcenter. When they double click the code in Teamcenter (see CodeFromTeamcenter.jpg) it opens in whatever the default viewer for the computer is, for them, it is a CNC code editor.

CodeFromTeamcenter.jpg

When they double click the same bit of code in the Teamcenter Navigator in NX (see CodeFromNX.JPG) , it opens the code in the standard information window, which adds additional header information.

CodeFromNX.JPG

 

Because the machine shop prefers not to go back and forth from NX and Teamcenter, they would like to stay within NX, and have the code open in the CNC code editor. Is this possible? and if so, what needs to be changed?

-Dave
NX 11 | Teamcenter 11 | Windows 10

Learn online





Solution Information