Cancel
Showing results for 
Search instead for 
Did you mean: 

M114 TNC command CSE Simulation

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi, 

 

Is TNC command M114 included in CSE simulation parser. 

 

How can I reproduce its functioning?

 

Best Reagards

Ivan

4 REPLIES

Re: M114 TNC command CSE Simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello M114 is not part of the OOTB TNC.CCF

 

To add it I would give it a try if reusing M128 for it will do this already.

To do so copy the M128 into your MCF and rename it to M114.

 

There are some minor differences between M114 and M128, but give it a try it may solve you need already.

 

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: M114 TNC command CSE Simulation

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi Thomas, 

 

I can´t copy M128 to current file. I´m not alowed do do this in this kind of commands. 

 

How could you do it from the begining?

 

Best Regards

Ivan

Re: M114 TNC command CSE Simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

Make sure you have select the correct source. Which NX version you are running? This it what you should see.

 

2017-03-24 14_27_16-Machine Configurator - [D__Siemens_NX11.0.0_MACH_resource_library_machine_instal.png

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: M114 TNC command CSE Simulation

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi Thomas,

 

I have tried using M128 as M114. That simply does not work.

 

I don´t know very well how I can to do with this command beacuse I can´t edit "GMe_Set5AxisTransformation" Method. 

 

Maybe editing "GMe_SwivelingCalculateLinears" can I find a solution? 

 

Best Regards,

Ivan

Learn online





Solution Information