Cancel
Showing results for 
Search instead for 
Did you mean: 

MAIN & LOCAL

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I'm creating a 5-axis positioning post that needs the XYZAB relative to MAIN at the first rapid and then the motion of the operation be relative to LOCAL. (There's a sub call at the start of the local motion that works like a G92). I think I can trap mom_csys_matrix to get MAIN coords while the operation is in the LOCAL mcs but I'm not sure how to convert them into mom_pos(0-5).

The motion during the operation is only 3-axis, no rotary.

 

example:

(first rapid needs to be relative to MAIN)

G0 G54

X3.454 Y4.876  < these are the values I need

A25.3 B56.9      these are the values I need

Z1.2                    these are the values I need

 

SUB CALL - like a G92, (xyz's are now relative to the current position)

 

G1 Z-.01

X.002 Y.01

X.05 Y.03

X.. Y..

X..Y..

X..Y..

 

Do I do it in mom_before_motion?

How do I reset the kinematics?

 

 

1 REPLY 1
Highlighted

Re: MAIN & LOCAL

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not a direct answer to your question, but one thing I've noted is that if you change kinematics in the initial/first move events, the mom_pos values are still in the "old" kinematics setup (i.e they don't get changed)

 

One possibility is to use the mom_mcs_goto variable? 

 

Anyhow, mapping from one CSYS to another is "standard" matrix algebra - you should be able to Google the math you need.  And there are some MOM functions that should be useful search for "VEC3" - e.g. VEC3_unitize).

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information