Cancel
Showing results for 
Search instead for 
Did you mean: 

MCS FIXTURE OFFSET

Pioneer
Pioneer

In our program we use 6 different MCS fixture offset ;

 

from G54.1P1 to G54.1P6 but when we post it , output is like this from from G54 to G59 ,

 

How can i change G54 to G54.1P1 in postbuilder...

4 REPLIES 4

Re: MCS FIXTURE OFFSET

Phenom
Phenom

You will have to change the word G_offset to have a leader of "G54.1 P" and $mom_fixture_offset_value - 53 if offsets are entered in cam as 54 etc.

NX12.02
Windows 10 Pro

Re: MCS FIXTURE OFFSET

To make your fixture offsets more portable across machines, I would recommend using 1-6 in the MCS fixture offsets. Then in the post you can use "$mom_fixture_offset_value" or "$mom_fixture_offset_value +53", depending on how they are numbered on the control.

Mark Rief
Retired Siemens

Re: MCS FIXTURE OFFSET

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I second Mark's suggestion to start at 1 and work up.

 

Note with appropriate tcl code, you can support all sorts of ranges using the "1 thru n" scheme

- Okumas G15 Hn (n = 1 thru whatever)

- Fanucish "G54-G59" + "G541. Pn"

- Siemens (I forget exactly, but something like) "G54-G56" then "G503 thru ..."

 

Ken

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Re: MCS FIXTURE OFFSET

Phenom
Phenom

We have done this as standard as well (1 based) since we have about every control and setup.

NX12.02
Windows 10 Pro

Learn online





Solution Information