Cancel
Showing results for 
Search instead for 
Did you mean: 

MCS - Purpose: Local - Special Output: None

Genius
Genius

Hello,

 

Could anyone please explain the behavior and effects of using a local MCS with Special Output set to None?

 

The NX CAM help states: Bases the output on the local MCS coordinates

 

Does anyone know more to this?

Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5
1 REPLY 1

Re: MCS - Purpose: Local - Special Output: None

Gears Phenom Gears Phenom
Gears Phenom

I just see these variables:

mom_special_output 0 1 2 3  (none0, fix. offset 2, use main1, csys rot3)

mom_coordinate_system_purpose 0 1 (local, main)

mom_kin_coordinate_system_type (local, main, CSYS (when rot))

- maybe this is only strings and you can use them whatever you want? I dont know.

 

and output of these variables is mysterious to me:

mom_sys_coordinate_system_status

mom_kin_coordinate_system_status

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information