Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

MCS has to be clicked to update assoiative position

Experimenter
Experimenter

Iam using "Z-axis, Y-Axis and origin" as method to position the MCS. The Y-axis uses "2 Points" to find its correct position. When updating the model, the Y-axis position doesnt change immediatly. It has to be clicked in the "Geometry viewer" to be updated to the new position. After being clicked, it finds the correct position. Is it possible to have the MCS automatically update its orientation without needing to click it?

 

Iam using

NX 11.0.0.33 MP4

4 REPLIES

Re: MCS has to be clicked to update assoiative position

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The display of the MCS is only updated on demand, its display doesn't update instantly like the WCS.

This is the case for all CAM objects, so you will have to create an enhancement request at GTAC for an instant update.

In addition, which of the many possible MCS objects would you like to have the display updated automatically?

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: MCS has to be clicked to update assoiative position

Valued Contributor
Valued Contributor

Which to highlight automatically?

In this order

 

The parent MCS of any CAM feature selected. 

The first MAIN MCS found in the Geometry tree or the First MCS in the tree.  For us it is the same thing.  (this would be the one when the part opens.)

 

Having the MCS hanging somewhere in space when opening CAM parts is confusing.   Just spent an hour with a user going over this very point.   

 

 

Re: MCS has to be clicked to update assoiative position

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I agree  - either the MCS of a selected object, or the first MCS found.

 

It is **BAFFLING** to users when they open a part and the MCS displayed DOES NOT CORRESPOND TO *ANY* MCS IN THE PART!!!!!!!!

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: MCS has to be clicked to update assoiative position

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@ohjert there needs to be an enhancement request created at GTAC. When you get an ER number, post the number and the text of the ER here and we can request to get linked to it to increase the customer count.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information