Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

MCS

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

I have put four MCS (G54,G55,G56,G57) in Nx.

But the output is wrong.

For first operation I have G54, but output si G57.

Next operation doesn´t have nothing (without tool change).

Third operation is ok.

And fourth operation is OK.

Can someone help me?

 

5.JPG3.JPG

6 REPLIES 6

Re: MCS

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Without knowing what code is in the post processor to output the fixture offset it would be impossible to answer your question.

 

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: MCS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

1) What does the geometry view look like?

2) How are the MCS objects defined? (i.e. in "Details" block, what is set for "Purpose" and "Fixture offset", and, if purpose is not "Main", what is set for "Special output" settings in that block?)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: MCS

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
mom_fixture_offset_value

Re: MCS

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Purpose is LOCAL
G54 Fixture offset 1
G55 Fixture offset 2
G56 Fixture offset 3
G57 Fixture offset 4

Re: MCS

Legend
Legend

Make Initial and first move the same. Only one or the other is used.

 

Initial is used if there is a tool change.

 

First is used for every operation without a tool change. 

 

 

work offset.PNG

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Re: MCS

Siemens Genius Siemens Genius
Siemens Genius
I guess I should have ask what are you using to create a tool list at the beginning of your program? if you are using the "pb_cmd_tool_list.tcl" from the postbuilder custom commands folder you may need to check the "PB_CMD_save_active_oper_tool_data" and make sure you are saving the fixture offset variable, because what happens is as it cycle through the tools it uses the fixture offset from the last tool.
Frank Bartucci
NX CAM COE

Learn online





Solution Information