Cancel
Showing results for 
Search instead for 
Did you mean: 

MENCMachining Item type in Teamcenter

We are trying to use MENCMachining Item type in Teamcenter. I was able to get all of our posts to work to use this Item type to save our posts and Shop docs back into teamcenter except one.

I added the following line to the .dat fiel and everything works.

LIBRARY_CAM_OUTPUT,${UGII_CAM_LIBRARY_TEMPLATE_DIR}cam_output.def,${UGII_CAM_LIBRARY_TEMPLATE_DIR}cam_output.tcl

 

The one I can't get to work is a DMG machine which we get a Machine Kit for. I'm not sure how to get this one to work so it saves back to teamcenter the Post and Shop Docs.

 

Looking for some help or guidance.

 

THanks

Steve

 

3 REPLIES 3

Re: MENCMachining Item type in Teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Does the posted file (NC code) file extension (.ptp or .eia or whatever) match one of the ones expected by TC?

Try

- posting

- manually rename output file (in %TMP% folder) with .PTP extension

- see if it imports back into TC

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: MENCMachining Item type in Teamcenter

I tried that and it didn't work Ken.

Re: MENCMachining Item type in Teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is the output written to a special place?

To automatically upload the files into Teamcenter they need to be placed into the export folder. This is usually the default location in managed NX, so your PP must move the file somewhere else.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information