Cancel
Showing results for 
Search instead for 
Did you mean: 

MKE didn't support ipm as Cut unit?

Genius
Genius

My process to duplicate issue.

1. I used Teach Operation Set to teach MKE my machining knowledge.

1.png

2. I create Feature process for my mapped feature

2.png

3. I check my feeds and speeds Cut is 0 ipm. Approach is rapid which is not as I set in the example(step4).

3.png

 

4. In the example operation, I teach NX  the Cut is 18ipm, and approach is 30 ipm as shown below

4.png

5.So I go to my MKE, I found that everything is messed up, it looks like MKE didn’t support ipm as the unit

5.JPG

1 REPLY 1

Re: MKE didn't support ipm as Cut unit?

Genius
Genius

I just tried both English and metric  MKE template.  It shows that the feeds rate is always written in "mmpm", only the feed valus are correct. So I am thinking the MKE developer may just use mmpm as a generic unit for simple coding. If it is english enviroment it will output ipm, if it is metric enviroment it will output mmpm. 

 

Learn online





Solution Information