Cancel
Showing results for 
Search instead for 
Did you mean: 

MKE expression for Solid Profile 3D

Valued Contributor
Valued Contributor

Hello I would like to express this setting for the Solid Profile 3D in the MKE.

 

snip_20171013114604.png

I have teached this operation but the setting of the Smoothing did not transferd to the MKE.

Do I have to set this in the Add-Ons?

 

Hope for you help, thank you.

 

NX 11.0.1.11
1 REPLY 1

Re: MKE expression for Solid Profile 3D

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

The MKE operation customization (i.e. the supported set of operation parameters) has to be maintained manually unfortunately. This means that new operation parameters that get added to an NX CAM operations don't automatically show up in the MKE. It requires a bit of work on our side.

 

In situations like this, it's recommended that you double check the MKE customization. In the case of the Solid Profile 3D operation the NX Dailog column for the Cutting Parameters -> Corners dialog doesn't show any Smoothing parameters.

Solid_profile_3d_customization.png

 

 

 

 

 

 

 

 

 

 

 

 

 

 

We'll need to add them to the customization_base.xml file.

Please send me a personal message if you would like to receive an updated version of this xml file which will give you access to these missing parameters.

 

Tom van 't Erve

NX CAM Development

Learn online





Solution Information