Cancel
Showing results for 
Search instead for 
Did you mean: 

MKE function for Percent of Flat Diameter

Valued Contributor
Valued Contributor

Hi,

 

I want to define a "Percent of Flat Diameter" in my MKE but I cannot find a function to

define a value. When I generate my teached operation (Floor Wall IPW) I always get the value 75.

 

snip_20170830131340.png

 

 

 

NX 11.0.1.11
1 REPLY

Re: MKE function for Percent of Flat Diameter

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

Your screenshot seems to indicate that your focus is on the stepover for a Floor Wall operation.

For that, you will need to create an Add-on of type Stepover and class Percentage_Tool_Flat:

Stepover_add_on.png

 

 

 

 

 

 

 

 

 

 

 

 

 

 

You specify the value (e.g. 75%) in the Add-on condition:

 

Stepover_add_on_condition.png

 

 

 

Tom van 't Erve

NX CAM Development

Learn online





Solution Information