Cancel
Showing results for 
Search instead for 
Did you mean: 

MOM_TCL: Can not open TCL script file.

Experimenter
Experimenter

Hey Everyone,

        

             I am new to this forum and NX as well. I am currently trying to edit cutting parameters in the operation navigator - program order. Everytime I right click a operation and hit edit a message pops up saying "MOM_TCL: Can not open TCL script file." and I'm not sure what that is telling me. im hoping someone has experience with this and can point me into a few possibilities. I'm using NX9 and TC10

 

Kind Regards

2 REPLIES

Re: MOM_TCL: Can not open TCL script file.

Gears Phenom Gears Phenom
Gears Phenom

1 did you edit some files or is it a new isntalation without any editing? (templates, ude, etc..)

2 check the logfile

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: MOM_TCL: Can not open TCL script file.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I forget in NX9, but the log file is either "File" -> "Help" -> "Log file"

Or "Help" -> NX log file

 

Or something like that.

Scroll ALL the way to the bottom

start scrolling up & see if there is a more intelligable error message.

 

If you want, you could post the log file here, BUT MAKE SURE to strip off the site ID & webkey access code info at/near the top!

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information