Cancel
Showing results for 
Search instead for 
Did you mean: 

MOM_TCL error while running ISV simulation

Pioneer
Pioneer

Hi all, 

I have build ISV setup for EDM machine(Fanuc CSE drivers used).The machinehas a very different kind of controller.The subprograms are getting output in the main program and called by GOTO statements.

 

I am able to run the simulation completly but at the end of the operations it will give MOM_tcl erro attached here in.The log file is also attached here in.

 

Can anybody suggest me what should I look for to remove this errror.

 

Regards

Keerti

2 REPLIES 2

Re: MOM_TCL error while running ISV simulation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

actual error is out of the screenshot which you attached. It will be on the end of that long line.

It would be easier if you just paste those lines here.

My guess is that file can't be found.

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: MOM_TCL error while running ISV simulation

Pioneer
Pioneer

Hi ALL, 

 

I just got the resolution.I was using suprogram so in post it is opening file and closing file to rite the subprograms and it seems ISV will read that internally and hence we need not call that proc in post but it shud exist in post I believe.

 

The ISV is working for me now.

 

Keerti

 

Learn online





Solution Information