Cancel
Showing results for 
Search instead for 
Did you mean: 

MOM_display_message possible in new Translation-Files in NX10?

Valued Contributor
Valued Contributor

Is it possible to translate messages from "MOM_display_message" with the new translation-files in NX10 (...localization\translations\german\xxx_german.txt)? If yes, which file do I have to customize?

Werner
Production: NX10.0.3, FBM | TcUA 10.1.2.2
Development: VB.NET, Tcl/Tk | Testing: NX12.0
1 REPLY

Re: MOM_display_message possible in new Translation-Files in NX10?

The messages from the post use the standard NX localization process, so they should be displayed in the local language.

 

I think the issue you are asking about is adding your own text strings to the localization database, and I don't think there is a way to do that. If this is important for you, I would contact GTAC and enter an ER.

 

All those files you see are part of our new localization architecture, not for your customization ;*)

Mark Rief
Retired Siemens

Learn online





Solution Information