Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

MOM_run_postprocess

Genius
Genius

When using the MOM_run_postprocess command, is it possible to use a sub-post that is located in a different directory than the main post.

Mike Diamond, CNC Programmer, Orizon Aerostructures Inc.

Production: NX10.0.3.5, Vericut 7.4.1, ICAM V21
Development: VB.NET, Tcl/Tk
Testing: NX11
1 REPLY 1

Re: MOM_run_postprocess

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Yes.
Just use full directory path to def and tcl file

 

You can also use "UGII directiories", like for example: ${UGII_CAM_LIBRARY_MACHINE_DIR}my_machine\postprocessor\

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Learn online





Solution Information