Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

MP(Maintenance Pack) output

Valued Contributor
Valued Contributor

Hello.

Is there a way to get the MP(Maintenance Pack) level on the same line as the NX version….?

 

MOM_output_literal "(NX VERSION   : ${mom_ug_version})"

 

 

Current posted output...

(NX VERSION        : NX 9.0.3.4)

 

 

Desired posted output...

(NX VERSION        : NX 9.0.3.4 MP12)

 

 

Kal.

NX 9.0.3.4 MP12 | PB 9.0.3.2 | NX11.0.2.7 MP13 | PB 11.0.2 | VERICUT 7.3.4
20 REPLIES 20

Re: MP(Maintenance Pack) output

The only way I know of is using an API program to parse the syslog. See https://community.plm.automation.siemens.com/t5/NX-Programming-Customization/Get-current-NX-Version-...

Mark Rief
Retired Siemens

Re: MP(Maintenance Pack) output

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Below find some Tcl code that I use as a custom function in MKE to determine the exact NX release.

    global HAI_current_NX_release

    set outputFile [file nativename "[MOM_ask_env_var UGII_TMP_DIR]\\env_print_out.txt"]
    set HAI_current_NX_release ""

    exec "[MOM_ask_env_var UGII_ROOT_DIR]\\env_print.exe" -m >$outputFile

    if { [file exists $outputFile] == 0 } {
      exec "[MOM_ask_env_var UGII_ROOT_DIR]\\env_print.exe" -n >$outputFile
    }

    if { [file exists ${outputFile}] == 1 } {
      set fileHandle [open $outputFile]
      set HAI_current_NX_release [read $fileHandle]
      close $fileHandle
    }

    set PosComma [string first "," $HAI_current_NX_release]
    if { $PosComma > 0 } {
      set HAI_current_NX_release [string range $HAI_current_NX_release 0 [expr $PosComma - 1]]
    } else {
      set HAI_current_NX_release [string trim $HAI_current_NX_release]
    }

    MOM_log_message "Current NX Release ... $HAI_current_NX_release"
Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: MP(Maintenance Pack) output

Phenom
Phenom

If you wish to redirect exit status on a variable, without passing by opening a file. You can make like that also :

set NXversion_number [exec $env(UGII_ROOT_DIR)env_print.exe -n]
set NXpatch [exec $env(UGII_ROOT_DIR)env_print.exe -m]

 

Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com

Re: MP(Maintenance Pack) output

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note there is an existing ER 7915944 (Stefan?) to get this MP info as an ENV variable (similar to UGII_FULL_VERSION)

 

I have an IR 7916250 (closed as a duplicate to IR  7916249) to have ENVs that include Hotfix / patch info as well.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: MP(Maintenance Pack) output

Valued Contributor
Valued Contributor

Thank you all for your contributions....

Stefan's cc is what I ended up using.  Thanks Stefan!Smiley Happy

 

Kal.

NX 9.0.3.4 MP12 | PB 9.0.3.2 | NX11.0.2.7 MP13 | PB 11.0.2 | VERICUT 7.3.4

Re: MP(Maintenance Pack) output

Thanks @Stefan_Pendl - very clever. I was not aware of the -m switch for env_print.

In NX11 there is no more UGII_ROOT_DIR, so I changed those references to UGII_BASE_DIR\\ugii:

 

 

    exec "[MOM_ask_env_var UGII_BASE_DIR]\\ugii\\env_print.exe" -m >$outputFile

 

 

 

 

 

Mark Rief
Retired Siemens

Re: MP(Maintenance Pack) output

Valued Contributor
Valued Contributor

Stefan,

Some of my colleagues, no MP on their computers, when they post, NX base version does not show...any ideas how to fix this?

 

; POST PROCESSOR   : GROB-G550
; PROGRAMMED BY  : Bugs Bunny
; NX VERSION            :
; DATE                         : Mon Feb 13 15:06:46 2017

 

 

Kal.

NX 9.0.3.4 MP12 | PB 9.0.3.2 | NX11.0.2.7 MP13 | PB 11.0.2 | VERICUT 7.3.4

Re: MP(Maintenance Pack) output

Did you use all of @Stefan_Pendl's tcl sample, or just the env_print -m command? The sample first tries -m to get the HFor MP. If that is null, then it uses -n to get the release. 

Mark Rief
Retired Siemens

Re: MP(Maintenance Pack) output

Valued Contributor
Valued Contributor

Mark. Used the entire code...

NX 9.0.3.4 MP12 | PB 9.0.3.2 | NX11.0.2.7 MP13 | PB 11.0.2 | VERICUT 7.3.4

Learn online





Solution Information