Cancel
Showing results for 
Search instead for 
Did you mean: 

Machine Configurator Controller file for Osai Series-10

Creator
Creator

I am looking for anyone with knowledge of creating a CSE .MCF for an Osai Series-10 controller.
Machine Configurator OOB does not appear to support this control.

Any suggestions or work arounds?

 

Thanks

 

Doug

8 REPLIES 8

Re: Machine Configurator Controller file for Osai Series-10

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I think a best way will be make CCF\MCF from FANUC base.

 

Example from OSAI 10

 

G27 G40 G71 G90
G94
G16XY
(TCP)
G0 G79 Z0
  
(DIS,"5AXIS_007_COPY")
G210 C5
G0 A0 C-90
(UAO,4)
(TCP,1) - exactly G43.4
(DIS,"VVEDITE DLINU INSTRUMENTA +212.540 I NAJMITE KNOPKU TCP ON")
M00
G291 w1 r-1 S18000.000  - w1 r-1 IGNORE
M03 - ALL BELOW - PURE FANUC
N1 G01 G90 X-212.785 Y-.239 A17.496 D0.0 F6000.
N2 Z29.663
N3 X-208.191 Z15.09
N4 X-207.315 Z12.312 F2000.
N5 X-207.278 Y-.151 Z12.193
N6 X-207.27 Y0.0 Z12.168
N7 X-207.283 Y-.057 Z12.212 A17.493 D-358.824
N8 X-207.297 Y-.114 Z12.257 A17.486 D-357.648
N9 X-207.31 Y-.17 Z12.304 A17.473 D-356.472
N10 X-207.323 Y-.227 Z12.351 A17.455 D-355.297
N11 X-207.335 Y-.284 Z12.399 A17.431 D-354.122
N12 X-207.347 Y-.34 Z12.447 A17.403 D-352.946
N13 X-207.357 Y-.397 Z12.492 A17.369 D-351.772

Re: Machine Configurator Controller file for Osai Series-10

Creator
Creator
Thanks for the info.



I'm working with a trial of M.C. and trying to make heads or tails of it.



I was told there wasn't much documentation or training help.



My initial thought was to use a Fanuc as I realize the similarities.



My post was a modified from a Sim05 Fanuc.





One of the problems is trying to figure out how to change a commented
line from (this is a comment line) to ;this is a comment line

After looking at the different .MCF files I am thinking it is in the
controller file.
This is where I'm at a loss.



I'm guessing I need to make a new command (TCP,1) and copy in the
code for G43.4



Thanks again for your insight.





Douglas A. Spitzer



Douglas A. Spitzer

Engineering Manager

Systems Administrator







1900 Lamar Court

Holland, Mi. 49010



voice: 616-395-5455

fax: 616-395-5457

Re: Machine Configurator Controller file for Osai Series-10

Creator
Creator

Can anyone tell me what defines the delimiters for a comment line in Machine configurator?

 

Thanks

Re: Machine Configurator Controller file for Osai Series-10

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

A lot of <CR> (Carrige Return) in your messages...

I think in your case will be useful CSE Method CSEPreprocessLine, this method is called for every NC Code line BEFORE the string is send to the parser, and you can substitute (TCP,1) to G43.4

replaceSubstr ("(TCP,1)", strLine, "G43.4")

Send me your e-mail, I will send you some explanation.

Yuri

 

 

 

Highlighted

Re: Machine Configurator Controller file for Osai Series-10

Creator
Creator

dspitz@formedsolutions.com

 

Thanks

Re: Machine Configurator Controller file for Osai Series-10

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

HI can you send me information about how to set up the  CSE Method CSEPreprocessLine

 

Thanks

 

ubaldo.garcia@idcae.com

Re: Machine Configurator Controller file for Osai Series-10

Creator
Creator

If you search for CSEPreprocessLine select CSEPreproc​essLine by Chigishev in Discussion Forum - NX Manufacturing

 

This will show how. You will need to create a new user defined method like shown above.

Re: Machine Configurator Controller file for Osai Series-10

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello,

 

I am having similar problem as Doug. I am trying to make Machine Configurator Controler for Osai 10. 

 

I am folowing your advice to use Fanuc controller as pattern for OSAI controller.

 

Now is main problem replacing G43.4 by (TCP) command. Can you please send me some more explanation about it?

 

Thank you.

 

Best regards,

 

Ondrej

Learn online





Solution Information