Cancel
Showing results for 
Search instead for 
Did you mean: 

Machine Kit with Teamcenter Integration without Resource Manager

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Experts,

 

We have a customer using Teamcenter rapid start (no Manufacturing or RM) and NX CAM.

The customer want to use machine simulation within Teamcenter but can't load machine in NX.

the INCLASS tcl procedure cannot be used to load the machine cause no classification is present

the ASCII tcl procedure do not load @db/machine_name/revision, while the machine is in TC.

 

Any suggestion?

 

Thanks

Fabrizio Bertoletti

 

 

1 REPLY

Re: Machine Kit with Teamcenter Integration without Resource Manager

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The following works for me in NX10

Create an item in Teamcenter the same name as the LIBRF in the machine_database.dat file.

 

E.g. for this line in machine_database.dat:

DATA|sim01_mill_3ax_fanuc_mm|MDM0101|3-Ax Mill Vertical|Fanuc|Example|${UGII_CAM_LIBRARY_INSTALLED_MACHINES_DIR}sim01_mill_3ax\sim01_mill_3ax_fanuc_mm.dat|1.000000|${UGII_CAM_LIBRARY_INSTALLED_MACHINES_DIR}sim01_mill_3ax\graphics\sim01_mill_3ax

Create the item "sim01_mill_3ax_fanuc_mm"

 

 

That is the top-level assembly file (with machine axes/etc. definition) of the machine model.

Then components can be any name, as they are found thru the assembly.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information