Cancel
Showing results for 
Search instead for 
Did you mean: 

Machine tool simulation

Siemens Creator Siemens Creator
Siemens Creator

How does Machine tool simulation compare to Software verification programs like Vericut? Does machine tool simulation verify the g and M code of the post processed file?

 

Thanks

3 REPLIES 3

Machine tool simulation is very similar to what you have...

Community Manager Community Manager
Community Manager

Machine tool simulation is very similar to what you have seen with applications like Vericut. It uses a solid assembly of the machine tool to show the motion of the machine as the NC program runs. It can be set up to simulate the internal toolpath records directly from NX. Or it can be set up to simulate the posted M- and G-codes (the final program that would be sent to the machine). There is an option to show the material removal as the machine simulates, or you can choose to simulate just the machine motion.

 

Hope that helps,

Derek Hart
... if we're not having fun, we're not doing it right!

Re: Machine tool simulation is very similar to what you have...

Experimenter
Experimenter

Where is the option to show material removal?

Highlighted

Re: Machine tool simulation is very similar to what you have...

In the Simulate dialog, Simulation Settings group, there is an option [] Show 3D Material Removal.

Mark Rief
Retired Siemens

Learn online





Solution Information