Cancel
Showing results for 
Search instead for 
Did you mean: 

Macro for postprocessing and not block NX?

Genius
Genius

Hi all,

 

Is there any possibility to create a macro, for postprocessing on NX and not block it, when it is postprocessing? Actually, I am using other postprocessor system, that you generate a CLSF file from NX CAM and you postprocess externally, so the NX is not blocked and you can work.

 

Thanks in advance.

2 REPLIES

Re: Macro for postprocessing and not block NX?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is the ability to batch process, but that will close the involved part file in NX.

 

You could use the RunUgPost batch script to post externally too.

 

BTW, I would not use a macro, since that is not update save and needs to be recreated with every change to a dialog in a MP, MR or major release.

The more convenient way is to use a journal, which is more update save and might only need a change with a major release change.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Macro for postprocessing and not block NX?

I am not sure I understand your question.

You can start a third party post outside of NX.

Are you trying to generate the CLSF in the background?

Mark Rief
Retired Siemens

Learn online





Solution Information