Cancel
Showing results for 
Search instead for 
Did you mean: 

Manufacturing General Setup Template error

Pioneer
Pioneer

When I open a part file and then go into file new and go to the manufacturing tab and select the General Setup. I set the name of the part I want it called and the reference part is specified, but when I click ok I get an error saying "An invalid file is specified, for a keywork.

See Syslog for details.

Anyone have any ideas.

3 REPLIES 3

Re: Manufacturing General Setup Template error

Pioneer
Pioneer

Sorted.

Re: Manufacturing General Setup Template error

Pioneer
Pioneer

I am having the same issue. Can you share the solution?

Re: Manufacturing General Setup Template error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Typically the file NX has issues with is listed in the syslog (File -> Help -> Log file)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information