Cancel
Showing results for 
Search instead for 
Did you mean: 

Manufacturing Machine Samples

Valued Contributor
Valued Contributor

Hello 

 

I would like to change the OOTB Machine Samples. Where can i change the path to those files?

2018-02-27_20h45_47.png

Is there a variable wich i need to set in the custom "Start.bat"?

 

Thank you for your assistance Smiley Happy

 


Production: {NX 10.0.3.5 MP18}
Testing: {NX 12.0.2.9 MP03}
2 REPLIES 2

Re: Manufacturing Machine Samples

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Bernhard_Swiss,

 

I guess what you want to do is adding a palette. The default Manufacturing Machine Samples can't be removed or changed.

 

It is fairly easy to create a new palette or point to a directory.


2018-02-27 22_23_53-.png

 

If the folder you added contains NX Part files, they will be shown as preview.

 

I made a video for you that shows how to add a folder as a palette:

(view in My Videos)

 

Cheers,

Alexander

Lead Product Manager - Mold & Die

Re: Manufacturing Machine Samples

Valued Contributor
Valued Contributor

Thank you for your answer and your video Smiley Happy

 

Unfortunately the palette can't be edited. Im woud like to use only the metric and my own machines in this existing folder.

But maybe this is an enhancement for the future to customize the existing pallets.

 

Im now trying to create a new palette using the video Smiley Wink 

 

 Greetings from Switzerlad


Production: {NX 10.0.3.5 MP18}
Testing: {NX 12.0.2.9 MP03}

Learn online





Solution Information