Cancel
Showing results for 
Search instead for 
Did you mean: 

Manufacturing Prefs

Gears Phenom Gears Phenom
Gears Phenom

CAM guys want me to change these defaults, but I haven't found them in the Customer Defaults area.. any clues?

 

ManufacturingPreferences.jpg

-Dave
NX 11 | Teamcenter 11 | Windows 10
4 REPLIES

Re: Manufacturing Prefs

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't think they are in the customer defaults (but I may be wrong).

 

In theory, there is an ENV (UGII_CAM_CONFIG) you can set to pull in the proper configuration file (which can pull in the proper template set file).

 

But I've had about 50% success in making it work.

 

Journals DO work well - maybe set one (or more) up on a ribbon that they can click?

 

Dim preferences1 As CAM.Preferences
preferences1 = theSession.CAMSession.CreateCamPreferences()
preferences1.ConfigurationFile = "C:\Folder_Path\my_cam_config.dat"
Dim nXObject1 As NXObject
nXObject1 = preferences1.Commit()
preferences1.Destroy()
Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Manufacturing Prefs

Gears Phenom Gears Phenom
Gears Phenom

I have UGII_CAM_CONFIG set correct now.

 

The other one eludes me...it also changes when I hit the reset to default, but when I hit apply, it changes back, WTH?

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Manufacturing Prefs

The template set is defined in the config file:

 

TEMPLATE_OPERATION,${UGII_CAM_TEMPLATE_SET_DIR}cam_general.opt

 

 

Mark Rief
Retired Siemens

Re: Manufacturing Prefs

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The dialog is not always displaying what is really used, it can't be used to check the current settings.

This is especially true when you use File => New setup parts, since the display is often different from what is used due to the CAM setup being used is the one saved with the template part.

 

You can use UGII_CAM_DEFAULT_TYPE_TEMPLATE and UGII_CAM_IMAN_TYPE_TEMPLATE to specify a default OPT file, if the one listed in the setup or the part file is not found.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information