Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Manufacturing multiplied parts in one process

Creator
Creator

Hi! I need Your help!

 

The first problem is:

 

I don't know how to multiply the same part and start manufacturing all of them using one piece of blank.Obviously I do know how to multiply object in modeling,I can take one object, do a patern but is there any posible to do this in Manufacturing? Sometimes I have different parts, I don't want to do this manually-I would like to choose a part, give an amount and that's it.

For example: I need ten cylinders d20x2 [mm],blank is 2mm thick.1.png

The second problem is more important to me- How can I make (here I don't know how to call this) bridge/support/this green thing ? I realy need this couse there is a lot of vibrations during the milling process, so these parts can not move. Here is better shot:

1.png

 

Thank You Smiley Happy

9 REPLIES 9

Re: Manufacturing multiplied parts in one process

Valued Contributor
Valued Contributor
on operations right click objet transform and choose direction x axis and
number of instances then highlight all ops and repeat once for y axis
toolmaker, Senior CAM engineer

Re: Manufacturing multiplied parts in one process

Creator
Creator

Ok, I got this ,thank You!!

 

So now how about these bridges/supports?

Re: Manufacturing multiplied parts in one process

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you asking how to make these tab supports automatically in the operation? That's not a current feature. You will need to model these in CAD and pattern them as you seem to have done already, or create boundaries with curves or points to use in the operation. Depending on the operation type you are using to cut the parts you will need to use either Check Bodies or Check Boundaries.

Re: Manufacturing multiplied parts in one process

Creator
Creator

You mean I should make manually this "bridge" like that?

For example.

2.PNG

I will try to make this as small and durable as it possible.

Re: Manufacturing multiplied parts in one process

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Does this need to be added to the part model?

Or the blank? 

or just as "check" geometry?

 

Particularly for mill-turns & lathes, I suggest users create a "manufacturing model"

This is an assembly of the engineering part, with the engineering part's solid body WAVE linked in.

Now you have a solid you can modify (add grind stock, or fillets/rounds/chamfers, or whatever - in your case, the green thing)

Then in your CAM (NC program) part, use the manufacturing model as the solid to machine.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Manufacturing multiplied parts in one process

Siemens Phenom Siemens Phenom
Siemens Phenom

You don't have to unite the bridge with the part you are cutting. Your first example of two different bodies was just fine. When defining your Workpiece in the Geometry View, simply select the round disk as the Part and then select the bridge body as the Check. The tool paths will avoid gouging both bodies, but you can specify different offsets for each. For example, you can rough out the Part (round disk) to 1.0mm full but cut the Check (bridge) to 0.0mm.

 

If these bridges are supposed to connect the part into the stock to use it as a sort of fixturing then you may need to model that as well and use it as the Check.

part_check.JPG

Re: Manufacturing multiplied parts in one process

Creator
Creator

I got this !

Thank You!

3.PNG

 

Is PLANAR PROFILE for this should be good? Please correct me Smiley Happy

 

Re: Manufacturing multiplied parts in one process

Siemens Phenom Siemens Phenom
Siemens Phenom

Planar Profile should be just fine if you simply want to cut around the part shape. The Check is defined as boundaries rather than a body, but it looks like you have that figured out.

 

To use the solids rather than boundaries you can try using Zlevel Profile.

Re: Manufacturing multiplied parts in one process

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

May be solid-profile-3D is an option for you too?

The operation you use highly depends on the input you have.

For example, if I want to machine a wall, but the path must follow the floor, I use flowcut multiple.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information