Cancel
Showing results for 
Search instead for 
Did you mean: 

Manufacturing - not entire machining area recognized

Experimenter
Experimenter

Hi !

 

I try to manufacture the hole below and have it already taught with the appropriate machining areas.

I called one of them " MIDDLE_FACES" (in orange on the picture). I would like to mill it in one operation, but it recognizes two surfaces separataly, instead of the one I taught.

 

Langloch_Fraesen.PNG

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Does anybody have any idea to fix the problem ?

 

Thank you very much !

NX 11.0.2.7

2 REPLIES 2

Re: Manufacturing - not entire machining area recognized

Legend
Legend

Hi!

 

It seems that your issue is due to the operation you intend to use. 

 

Have you tried it out with a Floor Wall or Cavity Mill operation?

Salvador Peregrina
Manufacturing Team Leader| NX 12.0.2

Re: Manufacturing - not entire machining area recognized

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

In order to give you best advice please send me the part on which you taught this feature.

On a side note:

This feature looks like a hole_obround_straight and should be recognized ootb.

What is the reason for teaching it yourself ?

Reinier Capelle
NX CAM Development - Customer Success

Learn online





Solution Information