Cancel
Showing results for 
Search instead for 
Did you mean: 

Max tool number?

Legend
Legend

I am not sure where to set the Max Tool Number. I set the MAX value for the T Address, but I still get an error in my warning.out file Tools all start at 1000 even though the max is 314. T20 would be T1020 for example. This is why the Leader is set to T1. I do not believe this is related to the max tool number issue though. I got the error before setting up the leader.


ADDRESS T
{
FORMAT Tcode
FORCE always
MAX 314 Warning
MIN 1 Warning
LEADER "T1"
}

Glenn Balon
Production: NX 12.0.2 MP4 Primarily CAM
5 REPLIES

Re: Max tool number?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi

Make sure you change both: Max value and T-word format

  

  Capture2.PNG

 

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Max tool number?

Legend
Legend

Had to change it manually in the .tcl file.

 

The post output was fine, it was just the warning message was that was erroneous.    

 

Untitled.pngmax_tool_number

Glenn Balon
Production: NX 12.0.2 MP4 Primarily CAM

Re: Max tool number?

Gears Phenom Gears Phenom
Gears Phenom

if you want to do it manualy - look into def file and look for your address.

 

example:


  ADDRESS G_cutcom
  {
      FORMAT      Digit_2
      FORCE       off
      MAX         999999999.9999 Truncate
      MIN         -999999999.9999 Truncate
      LEADER      "G"
  }

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Max tool number?

Legend
Legend

Even after changing in postbuilder, it reverts back to 32 for the mom_sys_max_tool_number after saving. 2017-10-25_0745.png

Glenn Balon
Production: NX 12.0.2 MP4 Primarily CAM

Re: Max tool number?

Gears Phenom Gears Phenom
Gears Phenom

Snímka.JPG

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information