Cancel
Showing results for 
Search instead for 
Did you mean: 

Mazak Integrex e-1060 Post

Experimenter
Experimenter

Does Siemens offer a post for a Mazak 5-axis Integrex e-1060?

 

Eric

6 REPLIES 6

Re: Mazak Integrex e-1060 Post

Phenom
Phenom

My guess is that they do - but maybe not since they are transitioning to "post configurator" posts. I think there are still siemens employees that make "postbuilder" ones too. These machines have a lot of capability. I would make sure that the post you get is:

1) Forward compatible (is open? require maintenance?)

2) Has all of these capabilities : turn, mill 5 axis, mill prismatic G68, G12.1 polar, XZC mode polar, cylindrical interpolation, on machine probing, lock axis and rotate udes functional.

You would probably be served best by a "kit" with CSE ISV with it (but this may be a little expensive.)

NX12.02
Windows 10 Pro
ITC Inc.

Re: Mazak Integrex e-1060 Post

Phenom
Phenom
Also make sure that B axis is functional on lathe. It is common to have to turn in (move B) while approaching internal turning for travel reasons.
NX12.02
Windows 10 Pro
ITC Inc.

Re: Mazak Integrex e-1060 Post

Phenom
Phenom
Oh - and support to flip the turning tools (flip tool around holder.)
NX12.02
Windows 10 Pro
ITC Inc.

Re: Mazak Integrex e-1060 Post

Experimenter
Experimenter

Thanks for the advise.

Eric

 

Re: Mazak Integrex e-1060 Post

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If I were you...

Create your own test parts.

Make sure to test EVERY operation/cut type you want the post to support.

Then make sure the posted output from your part runs crrectly on the machine.

Note (for reference) my test parts are typically:

- Turning: about 20 operations PER TURRET, PER SPINDLE (i.e. 2 turret 2 spindle = 80 operations)

- Milling (5 axis): about 150 operations if table-table.  200+ if tool rotates.  Add 50%-100% for 2nd spindle

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Mazak Integrex e-1060 Post

Experimenter
Experimenter
Hello Ken,

Thanks for your development suggestions.

Eric

Eric Pachulski
CNC Programmer
Sterling Engineering Corporation
236 New Hartford Rd
Barkhamsted Ct. 06063
Phone 860-379-3366 ext.127
E-mail : epachulski@sterlingeng.com

[Sterling Logo-Full Color]
This document, or attached documents or drawings, may contain technical data within the definition of the US International Traffic in Arms Regulations (ITAR) and is subject to the export control laws of the United States. Transfer of this technical data by any means to a foreign person or foreign entity per ITAR definitions, whether in the US or abroad, without a prior export license or other approval from the US Department of State is prohibited.

Learn online





Solution Information